FB#.STOREMULTITURN.BITS

Description

The number of most significant single-turn bits (power of 2 counts) used to determine if the position stored is valid after power cycle and ensures the motor did not move while the power was off.

Context

For more information on how to set FB#.STOREMULTITURN.BITS, see Store Multiturn.

Versions

Action Version Notes
Implemented 02-08-03-000  

General Information

Type

Read/Write

Units

N/A

Range

2-8

Default Value

2

Data Type

Integer

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported.

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

FB1.STOREMULTITURN.BITS

3500h

0eh

Unsigned8

-

-

Read/Write

No

FB2.STOREMULTITURN.BITS

3501h

0eh

Unsigned8

-

-

Read/Write

No

FB3.STOREMULTITURN.BITS

3502h

0eh

Unsigned8

-

-

Read/Write

No

FB4.STOREMULTITURN.BITS

3503h

0eh

Unsigned8

-

-

Read/Write

No

FB5.STOREMULTITURN.BITS

3504h

0eh

Unsigned8

-

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

FB1.STOREMULTITURN.BITS

30480

7710

Unsigned8

Read/Write

-

FB2.STOREMULTITURN.BITS

30481

7711

Unsigned8

Read/Write

-

FB3.STOREMULTITURN.BITS

30482

7712

Unsigned8

Read/Write

-

FB4.STOREMULTITURN.BITS

30483

7713

Unsigned8

Read/Write

-

FB5.STOREMULTITURN.BITS

30484

7714

Unsigned8

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

FB1.STOREMULTITURN.BITS

30480

Unsigned8

Read/Write

-

FB2.STOREMULTITURN.BITS

30481

Unsigned8

Read/Write

-

FB3.STOREMULTITURN.BITS

30482

Unsigned8

Read/Write

-

FB4.STOREMULTITURN.BITS

30483

Unsigned8

Read/Write

-

FB5.STOREMULTITURN.BITS

30484

Unsigned8

Read/Write

-